2021-04-08 3:37 PM
Hi,
I just upgraded my STM32CubeProgrammer to 2.7 and now getting error that can't find tf-a-stm32mp157c-dk2-serialboot.stm32.
I tried this on three other images that have worked in past, get same error.
tf-a-stm32mp157c-dk2-serialboot.stm32 is not found on file system for any of these images.
Specifics:
target: stm32mp157c-dk2
host: Windows 10
Images built on WSL.
Unfortunately I deleted 2.4 before installing 2.7, also tried 2.6, 2.5 and get same problem.
Have any suggestions ?
Solved! Go to Solution.
2021-04-10 8:34 AM
Well….. I think I sorted it out. It looks like STM32CubeProgrammer does not support symbolic links in WSL. This is something I knew of a couple years back and had script to run after build to remove symbolic links. This script got deleted and I totally forgot about why I needed it.
2021-04-08 7:48 PM
Following instructions here, https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#Preparing_the_USB_serial_link_for_flashing
I'm not seeing a response when running Bootloader.bat when running it in Admin PowerShell. Just see quick flash of application window.
Also, don't see DFU in device manager list.
Could this be contributing to the issue?
2021-04-08 7:56 PM
Update:
I do see the USB device show up in Universal Serial Bus Device as DFU in HS Mode @ Device ID /0x500, .....
So it's finding the USB device.
Documentation may be out of date, does not show this correctly.
2021-04-10 8:34 AM
Well….. I think I sorted it out. It looks like STM32CubeProgrammer does not support symbolic links in WSL. This is something I knew of a couple years back and had script to run after build to remove symbolic links. This script got deleted and I totally forgot about why I needed it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.