STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeIDE 1.13.0 released

STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch. What is new in 1.13.0? Added the support for new microcontrollers in the STM32U5 seriesAdded the support for new microcontrollers in the STM32WBA seriesAdded the sup...

Resolved! GTK apps missing libraries

Hi.I started to play with STM32MP1 micros and have a problem. How can I add so libraries not having "normal" linux tools? I wrote a simple GTK app and I am missing libpcreposix.so.0 

pj_stm by Associate III
  • 2888 Views
  • 2 replies
  • 0 kudos

Resolved! Reading and writing RAM via ST-Link

I am using STM32MP153 MPU on custom board.Is it possible to read/write memory region using ST-Link connected via JTAG interface?Most interesting if this is possible through some command line interface, perhaps my own C program using some API.

axel101 by Associate III
  • 5644 Views
  • 6 replies
  • 0 kudos

STM32MP157 in KEIL error.

Hello.I use a board STM32MP157A-DK1. I have SD-card with linux and now i try to run the board in KEIL. I have read file "Using STM32MP1 Cortex-M with Keil MDK". But I get error:Error: flash download failed.Also a can see:Full ship erase done.No Algor...

DFomi.1 by Associate II
  • 8035 Views
  • 14 replies
  • 0 kudos

Wrong partition size and "Error while reading the file" while programming flash layout to STM32MP157

Hi,after changing some kernel settings probably, I suddenly can not flash it to our custom STM32MP157 based board. Process fails around 100% of last partition with error: "Error: Error while reading the file"Looks like Cube reads file size incorrectl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.