STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Modify debug load mode of stm32mp157f-dk2

I am using stm32mp157f-dk2 and followed https://wiki.st.com/stm32mpu/wiki/Getting_started with help of stmcubeIDE. I am able to debug M4 core and also see SWV prints with ST A7 image and M4 image. Both images are available through above ST web site. ...

_legacyfs_online_stmicro_images_0693W00000bjxDbQAI.png _legacyfs_online_stmicro_images_0693W00000bjxC9QAI.png _legacyfs_online_stmicro_images_0693W00000bjxCsQAI.png _legacyfs_online_stmicro_images_0693W00000bjxEFQAY.png
Kalpesh1 by Associate II
  • 2909 Views
  • 4 replies
  • 0 kudos

Resolved! stop after Run or Debug action

hello.Now I am using stm32mp157a-ev1 board and coding M4 program on stm32cubeide.However, there is a problem that the stm32cubeide stops at 70% after starting to run or debug.And can check the log for errors in metadata.2023-04-04 17:11:23,560 [INFO]...

0693W00000bhTiGQAU.png
KNam.2 by Associate II
  • 3238 Views
  • 4 replies
  • 0 kudos

Resolved! Failed to firmware upgrade ST-LINK firmware on STM32MP157F-DK2 board using STM32CubeProgrammer version 2.12

Hi,I am using STM32CubeProgrammer version 2.12 running on Windows 10 to connect to the STM32MP157F-DK2 board ST-LINK connector CN-11.I managed to connect and when I click "Firmware upgrade" the STLinkUpgrade 3.4.0 window opens.However, when I press "...

SThon.1 by Associate II
  • 3264 Views
  • 2 replies
  • 0 kudos

Resolved! undefined reference to `HAL_ADC_Init'

I've been trying for hours to read an analog value from a pin and write it over UART with no success on my STM32MP1. I've assigned PF14 to ADC2_INN2 and set IN2 to "IN2 Differential", then I generate the code and when I try to build I get a bunch of ...

msche.1 by Associate III
  • 5676 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.