STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

debugging problem(urgent)

how i can solve it : Error in final launch sequence: Failed to execute MI command:target extended-remote localhost:3333 Error message from debugger back end:Truncated register 16 in remote 'g' packetFailed to execute MI command:target extended-remote...

Resolved! STM32MP2x pinmux support in CUBEMX

Hello     We are planning to work on STM32MP2x processors in our custom design boards. We tried with latest version of CUBEMX for pinmux but it's not available. So, we would like to know when we can expect the pinmux support for STM32MP2x processors....

Resolved! "Unable to get the associate alternate setting of partition ID: 0xf1..." error after migrating to Windows 10 Host PC

USB speed  : High Speed (480MBit/s)                                 Manuf. ID  : STMicroelectronics                                  Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAB Re  v.Z,               ...

ASkri.1 by Senior
  • 6240 Views
  • 8 replies
  • 0 kudos

Resolved! How to enable 3 USB ports on STM32MP1

According to different STM32MP1 documentation such as STM32MP1-Peripheral-USB_Host_interface_USBH or STM32MP1-Peripheral-USB-On-The-Go-Full-and-HighSpeed-interface presentation there is two USB phy, one dual port HS phy and one single port FS phy. In...

PGE by Associate III
  • 5669 Views
  • 6 replies
  • 0 kudos

Yocto STM32MP157 DK2 - Display not working

HelloI use https://github.com/STMicroelectronics/meta-st-stm32mp with the stm32mp15-disco machine.It boots fine, I can access the shell via USB-UART. But the display just shows an STM Logo from the Bootloader. What do I need to change, so the display...

kbch by Associate III
  • 3862 Views
  • 4 replies
  • 0 kudos

Create new project in MX with STM32MP13

I have STM32CubeMX Version 6.10, STM32CubeIDE Version: 1.14.1with installed BSP STM32Cube_FW_MP13_V1.0.0When I create new bare project starting from evalboard STM32MP135F-DK as bare metal projectthen select NETXDUO, THREADX in Middleware and Software...

ravo_0-1710926926321.png ravo_1-1710926945424.png
ravo by Senior
  • 1612 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.15.1 released

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download. Main issues fixed in this patch: Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.