2024-04-29 4:31 PM
Hello
I use https://github.com/STMicroelectronics/meta-st-stm32mp with the stm32mp15-disco machine.
It boots fine, I can access the shell via USB-UART. But the display just shows an STM Logo from the Bootloader. What do I need to change, so the display works in Linux?
This is the error when trying to start X:
root@stm32mp15-disco:~# startx
xauth: file /home/root/.serverauth.724 does not exist
X.Org X Server 1.21.1.8
X Protocol Version 11, Revision 0
Current Operating System: Linux stm32mp15-disco 6.1.28 #1 SMP PREEMPT Thu May 11 14:04:52 UTC 2023 armv7l
Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
Current version of pixman: 0.42.2
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.0.log", Time: Fri Mar 9 21:17:20 2018
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
(EE)
Fatal server error:
(EE) no screens found(EE)
(EE)
Please consult the The X.Org Foundation support
at http://wiki.x.org
for help.
(EE) Please also check the log file at "/var/log/Xorg.0.log" for additional information.
(EE)
(EE) Server terminated with error (1). Closing log file.
xinit: giving up
xinit: unable to connect to X server: Connection refused
xinit: server error
2024-05-03 5:19 AM
Hi @kbch n
Can you please share version you are using and all details about yocto build config ?
Thanks
Olivier
2024-05-03 5:58 AM
I'm using this branch of the meta repo, commit 5e5b99ba054276d10b4afec2b80962de3455b0a1
➜ meta-st-stm32mp git:(mickledore) ✗ git status
On branch mickledore
Your branch is up to date with 'origin/mickledore'.bblayers and machine config:
➜ conf cat bblayers.conf
# POKY_BBLAYERS_CONF_VERSION is increased each time build/conf/bblayers.conf
# changes incompatibly
POKY_BBLAYERS_CONF_VERSION = "2"
BBPATH = "${TOPDIR}"
BBFILES ?= ""
BBLAYERS ?= " \
/home/bmarty/mp1/poky/meta \
/home/bmarty/mp1/poky/meta-poky \
/home/bmarty/mp1/poky/meta-yocto-bsp \
${TOPDIR}/../meta-st-stm32mp \
${TOPDIR}/../meta-openembedded/meta-oe \
${TOPDIR}/../meta-openembedded/meta-networking \
${TOPDIR}/../meta-openembedded/meta-multimedia \
${TOPDIR}/../meta-openembedded/meta-python \
"
➜ conf cat local.conf | grep MACHINE | grep stm
MACHINE = "stm32mp15-disco"Do you need something else?
2024-05-03 7:02 AM
Hi @kbch ,
Which image ?
I understand that Startx may depends on X11 .. which is not supported in our distribution.
I guess you might have to check all startx dependences and manage to add them to your distribution.
Hope it help,
Olivier
2024-05-03 7:12 AM
I'm using a customized image based on core-image:
IMAGE_FEATURES += " \
dev-pkgs \
hwcodecs \
package-management \
x11-base \
"
IMAGE_INSTALL += "\
packagegroup-base \
packagegroup-core-base-utils \
packagegroup-core-boot \
packagegroup-core-full-cmdline \
packagegroup-core-tools-debug \
packagegroup-core-x11 \
${CORE_IMAGE_EXTRA_INSTALL} \
"
inherit core-image features_check
Can I somehow check within the Shell if the display got initialized to rule out any X11 specific issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.