2020-07-23 8:23 AM - last edited on 2023-07-11 9:34 AM by Kevin HUBER
According to different STM32MP1 documentation such as STM32MP1-Peripheral-USB_Host_interface_USBH or STM32MP1-Peripheral-USB-On-The-Go-Full-and-HighSpeed-interface presentation there is two USB phy, one dual port HS phy and one single port FS phy.
In my understanding I should be able to enable 3 USB host port, two HS and one FS.
I am using the STM32CubeMX tool but I am unable to enable such 3 ports. I am able to enable two HS port but I am unable to enable OTG port. If I disable one HS port I am able to enable OTG port. So it seems STM32CubeMX allows to enable only two ports at the same time.
Is this an issue of STM32CubeMX or it's a real limitation of the chip ?
Note, I have tried with different package with the same results
Many thanks in advance for any help
Solved! Go to Solution.
2020-07-23 9:14 AM
Hello,
This is a limitation in CubeMX, I confirm you could really use three host ports (2 x high-speed + 1 x full-speed).
You have to edit the device tree manually for this case. see https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_full-speed_OTG-2C_with_micro-B_connector
Notice that OTG host HW/driver has some limitations which make it not recommended to be connected to an USB Hub.
2020-07-23 9:14 AM
Hello,
This is a limitation in CubeMX, I confirm you could really use three host ports (2 x high-speed + 1 x full-speed).
You have to edit the device tree manually for this case. see https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_full-speed_OTG-2C_with_micro-B_connector
Notice that OTG host HW/driver has some limitations which make it not recommended to be connected to an USB Hub.
2020-07-23 11:58 PM
Ok many thanks for your clear reply
Any other known limitation ? Is there any documentation with all known limitation / issue ?
2020-07-24 12:15 AM
See ES0438: STM32MP151x/3x/7x device limitations
See also https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note
2020-09-03 7:49 AM
@PatrickF According to your link above default IOs for USB OTG in full-speed mode are PA11 and PA12. These are general purpose IOs, are they powered by VDD or VDD_USB ? As USB is 3.3V signals does-it work well also with 1.8V VDD powered STM32MP157 ?
Thanks in advance for clarification
2020-09-03 8:27 AM
PA11 and PA12 are specific IOs and supplied by VDD_USB (3.3V typ.) when used as OTG_FS data pins, VDD otherwise.
No issue regarding VDD=1.8V
2024-05-16 7:48 AM - edited 2024-05-16 5:10 PM
Hi,
I had a similar problem with kernel 6.1.28, but I managed to solve it.I now can use all three USB ports ( 2xHS + OTG_FS )
I had the following message when connecting the board in peripheral mode :
dwc2 49000000.usb-otg: Failed to exit L1 sleep state in 200us
Patch : https://lore.kernel.org/lkml/20201123090114.12641-4-amelie.delaunay@st.com/
From: Amelie Delaunay <amelie.delaunay@st.com>
To: Minas Harutyunyan <hminas@synopsys.com>,
Felipe Balbi <balbi@kernel.org>,
Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Cc: <linux-usb@vger.kernel.org>, <linux-kernel@vger.kernel.org>,
<linux-stm32@st-md-mailman.stormreply.com>,
Fabrice Gasnier <fabrice.gasnier@st.com>,
Amelie Delaunay <amelie.delaunay@st.com>
Subject: [PATCH 3/3] usb: dwc2: disable Link Power Management on STM32MP15 HS OTG
Date: Mon, 23 Nov 2020 10:01:14 +0100 [thread overview]
Message-ID: <20201123090114.12641-4-amelie.delaunay@st.com> (raw)
In-Reply-To: <20201123090114.12641-1-amelie.delaunay@st.com>
Link Power Management (LPM) on STM32MP15 OTG HS encounters instabilities
with some Host controllers. OTG core fails to exit L1 state in 200us:
"dwc2 49000000.usb-otg: Failed to exit L1 sleep state in 200us."
Then the device is still not enumerated.
To avoid this issue, disable Link Power Management on STM32MP15 HS OTG.
Signed-off-by: Amelie Delaunay <amelie.delaunay@st.com>
---
drivers/usb/dwc2/params.c | 4 ++++
1 file changed, 4 insertions(+)
diff --git a/drivers/usb/dwc2/params.c b/drivers/usb/dwc2/params.c
index 9e5dd7f3f2f6..92df3d620f7d 100644
--- a/drivers/usb/dwc2/params.c
+++ b/drivers/usb/dwc2/params.c
@@ -194,6 +194,10 @@ static void dwc2_set_stm32mp15_hsotg_params(struct dwc2_hsotg *hsotg)
p->host_perio_tx_fifo_size = 256;
p->ahbcfg = GAHBCFG_HBSTLEN_INCR16 << GAHBCFG_HBSTLEN_SHIFT;
p->power_down = DWC2_POWER_DOWN_PARAM_NONE;
+ p->lpm = false;
+ p->lpm_clock_gating = false;
+ p->besl = false;
+ p->hird_threshold_en = false;
}
const struct of_device_id dwc2_of_match_table[] = {
--
2.17.1
Here is a working device-tree allowing to use both USB in high-speed and OTG as full-speed:
/dts-v1/;
#include "stm32mp157c-odyssey-som.dtsi"
/ {
model = "Seeed Studio Odyssey-STM32MP157C Board";
compatible = "seeed,stm32mp157c-odyssey",
"seeed,stm32mp157c-odyssey-som", "st,stm32mp157";
aliases {
ethernet0 = ðernet0;
serial0 = &uart4;
};
chosen {
stdout-path = "serial0:115200n8";
};
};
&dcmi {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&dcmi_pins_b>;
pinctrl-1 = <&dcmi_sleep_pins_b>;
};
ðernet0 {
status = "okay";
pinctrl-0 = <ðernet0_rgmii_pins_a>;
pinctrl-1 = <ðernet0_rgmii_sleep_pins_a>;
pinctrl-names = "default", "sleep";
phy-mode = "rgmii-id";
max-speed = <1000>;
phy-handle = <&phy0>;
assigned-clocks = <&rcc ETHCK_K>, <&rcc PLL4_P>;
assigned-clock-parents = <&rcc PLL4_P>;
assigned-clock-rates = <125000000>; /* Clock PLL4 to 750Mhz in ATF/U-Boot */
st,eth-clk-sel;
mdio0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0: ethernet-phy@7 { /* KSZ9031RN */
reg = <7>;
reset-gpios = <&gpiog 0 GPIO_ACTIVE_LOW>; /* ETH_RST# */
reset-assert-us = <10000>;
reset-deassert-us = <300>;
};
};
};
&i2c1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c1_pins_a>;
pinctrl-1 = <&i2c1_sleep_pins_a>;
i2c-scl-rising-time-ns = <100>;
i2c-scl-falling-time-ns = <7>;
status = "okay";
/delete-property/dmas;
/delete-property/dma-names;
};
&sdmmc1 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc1_b4_pins_a>;
pinctrl-1 = <&sdmmc1_b4_od_pins_a>;
pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>;
cd-gpios = <&gpioi 3 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
disable-wp;
st,neg-edge;
bus-width = <4>;
vmmc-supply = <&v3v3>;
status = "okay";
};
&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&uart4_pins_a>;
/delete-property/dmas;
/delete-property/dma-names;
status = "okay";
};
&usbotg_hs {
compatible = "st,stm32mp15-fsotg", "snps,dwc2";
pinctrl-names = "default";
pinctrl-0 = <&usbotg_fs_dp_dm_pins_a>;
dr_mode = "device";
status = "okay";
};
&pinctrl {
usbotg_hs_pins_b: usbotg-hs-1 {
pins {
pinmux = <STM32_PINMUX('G', 12, ANALOG)>; /* OTG_ID */
};
};
};
&usbphyc {
status = "okay";
};
&usbphyc_port0 {
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
connector {
compatible = "usb-a-connector";
vbus-supply = <&vbus_sw>;
};
};
&usbphyc_port1 {
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
connector {
compatible = "usb-a-connector";
vbus-supply = <&vbus_sw>;
};
};
&vdd_usb {
regulator-always-on;
};
&vdda {
regulator-always-on;
};
&usbh_ohci {
phys = <&usbphyc_port0> ;
phy-names="usb2-phy";
status = "disabled";
};
&usbh_ehci{
phys = <&usbphyc_port0>, <&usbphyc_port1 1>;
status = "okay";
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.