2022-05-04 6:11 AM
I am debugging a STM32MP1 boot but the bootrom does not manage to boot the FSBL from the SDMMC interface.
I extracted the traces and ran the bootrom trace analyzer script. However, some of the error messages contain error codes for which I could not find an explanation.
The relevant lines are:
< @ 00981105 | [ERR ] - SD_OverallRetryCnt ( 0x00000003 ) >
< @ 00981491 | [ERR ] - SD_InitDetailedErrorDesc ( 0x00000029 ) >
< @ 00981907 | [ERR ] - SD_InitFailed >What do the hexadecimal codes mean (the 0x00000003 and 0x00000029)?
In case it is needed, the full output from the script is attached.
Thank you for your help
2022-05-04 7:11 AM
HI @bfh_dls
value in parenthesis are not always error codes, but rather various parameters for more deep analysis by our internal team if needed.
For instance, here "( 0x00000003 )" shows that 3 retries has been done.
or later "BOOTCORE_HseFrequencyDetected ( 0x00000018 ) " reflect that 24MHz (0x18=24 decimal) has been detected on HSE.
On my side, I have not enough information for the "( 0x00000029 )" meaning.
But as the Bootrom.log file you share is exactly the same I got on one of our board (e.g. STM32MP157F-DK2) with no SD-Card connected. I suspect a more basic issue.
Please check:
Btw, did you use level translator between STM32MP15x and SD-Card (e.g. to support UHS-I) or a simple and direct connection ?
If you still have issue, maybe worth to share your schematics.
Regards.
2022-05-04 8:23 AM
Thank you for your answer.
I confirmed that I get the same bootrom trace when using a demo board without SD card.
I don't have a level translator on my lines but an EMI filter (EMIF06-MSD02N16).
2022-05-04 8:58 AM
Hi,
Did you have a look to SD-Card signals as I proposed above ?
If no clock, there is likely an Hw issue as BootROM log show that the SD-Card trial is correctly done.
Looking at your schematics does not give much information to me.
As you use a SOM from a 3rd party (assuming this is a working module), you could double check your SOM pinout/schematics Vs the official baseboard documentation provided by the SOM maker.
Maybe worth to contact the SOM maker.
Regards.
2022-05-05 5:49 AM
Hi,
I may have found an issue on your schematics.
There is two different supply names: +3.3V and +3V3.
Please confirm both are connected together.
Regards.
2022-05-09 5:24 AM
Hi Patrick,
The +3.3V and +3V3 are indeed connected together, the naming will be fixed in the schematic to avoid confusion though.
I did test the SD card interface with an oscilloscope and did not get a signal. I will check the PCB in detail.
I will also try the SDcard interface without EMI protection to make sure it does not interfere with communication.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.