STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB Composite in STM32MP157c

I am struggling to achieve a USB gadget with Mass Storage + rndis.When i start each service alone everything works but when i am trying to start both of them i receive the following error:dwc2_hsotg_ep_enable: No suitable fifo foundAny suggestion how...

AKokk by Associate II
  • 4981 Views
  • 5 replies
  • 1 kudos

Resolved! On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with M4 only (& not A7)?

On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with core-M4 only (& not core-A7)? I am not quite sure if the wifi module 1dx (U8 on the kit) is controlled by A7 or M4?Anyways, I want to interface it with M4. So, can it be possib...

ANalg.1 by Associate II
  • 3100 Views
  • 2 replies
  • 0 kudos

Kernel panic during startup

Hi I built the linux kernel by following the steps on the stm32mpu wiki web. All default configuration except enabled earlyprintk. However, when I restart the system, it does not work any more.This is the error in boot log....[  0.349451] pps_core: L...

uouox by Associate II
  • 1818 Views
  • 1 replies
  • 0 kudos

Is there a way to use the B-LCDAD-HDMI adapter (bridge chip ADV7533) on the STM32MP157a-ev1 board

Hi @PatrickF​ I think the previous question reached the maximum number of replies, so I write a new one hoping I'm doing well.Here's my weston.ini[core] #modules=cms-colord.so shell=desktop-shell.so backend=drm-backend.so idle-time=0 repaint-window=1...

MBassi by Associate III
  • 1425 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.