2023-03-23 12:48 AM
Hi ~
I'm using STM32MP157C MPU with my custom board
and trying to modify u-boot for my board.
This wiki article has been describe about "Modifying the U-boot".
Adding simple log like the example works fine.
But, If I try to change u-boot prompt string using "make menuconfig"
it seems like that changed prompt string didn't apply.
How to solve it?
Thanks.
Solved! Go to Solution.
2023-04-14 2:44 AM
Hi,
I work with it a few days ago with stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 (zip file with kernel, FSBL, u-boot downloaded from ST)
1) Build standard configuration.
# my location of compiler
source /opt/st/OpenSTLinux/openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
cd u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2
export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts
make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE=stm32mp157c-dk2 all -j12In directory build/stm32mp15_defconfig is .config file
2) copy it to main boot directory (../../u-boot-stm32mp-v2021.10-stm32mp-r2)
run
make menuconfigmodify configuration, write it.
3) copy .config to ../u-boot-stm32mp-v2021.10-stm32mp-r2/configs as yourconfiguration_defconfig
end of name _defconfig is important!
after that clean system with
make mrproperand build your configuration with
make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=yourconfiguration_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE=stm32mp157c-dk2 all -j12Michal Jahelka
2023-04-12 6:02 AM
Hello @hochul yoo ,
I apologize for the delay in response.
Have you been able to solve your issue?
In your case, is it mandatory to use the Distribution Package?
Otherwise you can make a try with the Developer Package: https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Installing_the_OpenSTLinux_BSP_packages
and
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-04-14 2:44 AM
Hi,
I work with it a few days ago with stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 (zip file with kernel, FSBL, u-boot downloaded from ST)
1) Build standard configuration.
# my location of compiler
source /opt/st/OpenSTLinux/openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
cd u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2
export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts
make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE=stm32mp157c-dk2 all -j12In directory build/stm32mp15_defconfig is .config file
2) copy it to main boot directory (../../u-boot-stm32mp-v2021.10-stm32mp-r2)
run
make menuconfigmodify configuration, write it.
3) copy .config to ../u-boot-stm32mp-v2021.10-stm32mp-r2/configs as yourconfiguration_defconfig
end of name _defconfig is important!
after that clean system with
make mrproperand build your configuration with
make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=yourconfiguration_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE=stm32mp157c-dk2 all -j12Michal Jahelka
2023-06-19 4:48 AM
Hi,
To compelete the previous answer, you can also use savedefconfig to simplify your configuration, menuconfig generate a very long .config.
$> make menuconfig
$> make savedefconfig
$> cp defconfig to ../u-boot-stm32mp-v2021.10-stm32mp-r2/configs/<yourconfiguration>_defconfig
U-Boot use the Kconfig to configure its configuration,
But .config is overidde at each make command with Makefile.sdk, by using the content of defconfing directoty (UBOOT_DEFCONFIG=yourconfiguration_defconfig)
https://wiki.st.com/stm32mpu/wiki/Menuconfig_or_how_to_configure_kernel
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Kbuild
https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#Defconfig
Patrick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.