cancel
Showing results for 
Search instead for 
Did you mean: 

Succesfully bringup STM32MP135 with FMC NAND

EricD-IES
Associate

Hi,

 

Just now I have done bringing up a custom board for STM32MP133/ STM32MP135 with OpenST Linux, with kernel 6.2:

- The whole boot chain bring up from tf-a, uboot, kernel.

- Configure PMIC and support DDR test.

- Support FMC NAND, change flash partition layout.

- A/B FOTA ready Yocto build (with uboot)

- Total boot time is 30 seconds to access to ADB (android platform tool)

- Platform CAN bringup

- Integrate Quectel modem for network over LTE

If someone needs something related to this, I can help.

Best,

Eric

 

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @EricD-IES 

Thanks for your post ! :) 

Olivier 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.