2024-04-11 8:31 AM
Hi,
we've upgraded our build from 5.15 to 6.1 and now the OS does not get the mac address set in uboot environment through a script. If i check the environment i can correctly see the ethaddr set via printenv. Is there something i can do in kernel config or ethernet driver?
2024-04-15 9:11 AM - edited 2024-04-17 9:34 AM
bump
2024-04-22 11:42 AM
Bump
2024-05-09 8:13 AM
Possible that no one cares about this? I'm still on 5.15 because of this issue. Please help
2024-05-31 4:57 AM
Hi @GCici ,
Sorry to come late in this thread.
For sure ST care about your issue but we would need further information.
Can you update status on your side ?
When you said you change from 5.15 to 6.1 do you means only the kernel or the whole OSTL version including BSP ( TF-A, Uboot, OPTEE) . This is mandatory.
If you may share some logs about the issue it can surely help
Olivier
2024-05-31 6:56 AM - edited 2024-05-31 8:46 AM
Hello Olivier,
i mean the whole OSTL system, so TFA,UBOOT,OPTEE and kernel. which kind of logs do you need?
I can say ethaddr is correctly set in u-boot environment and it shows correctly when i type printenv. When the system has started the mac address on eth0 is different from the one set in uboot environment.
Cheers,
GC
2024-06-07 7:19 AM
Hi @GCici ,
Complete boot log would be good for some checks
Thanks
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.