STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Support for Murata 2BC CYW4373 chipset

I would like to use the Murata Wi-Fi/BT combo module 2BC on STM32MP1.Is it possible?If it is possible, I would like to know how to integrate 2BC on STM32MP1. I understand following.- Murata 1DX are mounted on STM32MP1 evaluation board.- Murata has th...

STM32MP1 FMC address pins

Hello!I have a MP1 board (STM32MP157), and i was wondering if one can have control over which individual pins are used when it comes to FMC. I want to use FMC for PSRAM, 8-bit data mode, but the pin that corresponds to FMC_A2 is already in use (PF2),...

Resolved! eMMC flashing with GPT partition table

Hi ST Community,I am trying to flash a eMMC with STM32CubeProgrammer, in a STM32MP157F custom board. I am using a GPT partition file and a img.I can see the system is creating partitions and flashing, but the structure is wrong for eMMC, so it does n...

Flyback_0-1698484449426.png Flyback_1-1698484522541.png
Flyback by Associate II
  • 5840 Views
  • 2 replies
  • 0 kudos

STM32MP1 Switch to Production Boot

I have a board where a secondary CPU can select the STM32MP1's boot mode.  On initial boot, the MP1 boots from NOR flash.  I can then send a command to the secondary CPU which switches the MP1's BOOTx pins to enable engineering boot and resets the MP...

DPade.1 by Associate III
  • 4751 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.