2021-03-10 10:18 AM
Hello,
I have done the modification in the device tree related to inclusion of usart3 as per 3.3.1 Activation of a USART or UART instance in https://wiki.st.com/stm32mpu/wiki/Serial_TTY_device_tree_configuration
&usart3 {
pinctrl-names = "default", "sleep", "idle"; /* pin configurations definition */
pinctrl-0 = <&usart3_pins_a>; /* default pin configuration selection */
pinctrl-1 = <&usart3_sleep_pins_a>; /* sleep pin configuration selection */
pinctrl-2 = <&usart3_idle_pins_a>; /* idle pin configuration selection */
status = "okay"; /* device activation */
};
in the dk2 dsi
, but after kernel booting , Banner seems stuck at ST and doesnt loads the full gui.
I need to connect to it for delta changes in the application and then pushing it to the board using scp but without gui loading I cant test further. Help please !
I can connect via minicom and see ttySTM1 up.
this is the boot log :
I confirm that without any modifications , js building and loading the kernel works fine and GUI loads up.
Tx,
2021-03-14 10:34 AM
on further investigating the logs I foudn this differene :
Thee are the logs in which the GUI doesnt loads and it says that there is a failure in the display controller probe. Is the display controller using these USART3 lines?
How can i use it safely or any othe rusart lines?
Please assist.
[ 2.945081] stm32mp157-pinctrl soc:pin-controller@50002000: pin PI10 already requested by 4000f000.serial; cannot claim for 5a001000.display-controller
[ 2.957321] stm32mp157-pinctrl soc:pin-controller@50002000: pin-138 (5a001000.display-controller) status -22
[ 2.967113] stm32mp157-pinctrl soc:pin-controller@50002000: could not request pin 138 (PI10) from group PI10 on device soc:pin-controller@50002000
[ 2.980352] stm32-display 5a001000.display-controller: Error applying setting, reverse things back
[ 2.989501] stm32-display: probe of 5a001000.display-controller failed with error -22
Thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.