STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In ST-Link32 Utility, Read Out Protection is Disabled, but I get the errors: The elf loader Program function fails. Memory-Loader error Error occured during program operation Programming error @ 0x08000B60!

I have the latest version of ST-Link Utility (ver. 4.6.0) on Windows 10 and the latest firmware (V2.J37.S7), both of which I downloaded yesterday. My co-worker has ST-Link Utility ver. 3.7.0 on Windows 7 and firmware V2.J24.S7 and he has no trouble...

KLock.2 by Associate II
  • 1510 Views
  • 1 replies
  • 0 kudos

Hello I'm trying to write a loadable kernel module driver. I get an error during compilation: ERROR: modpost: "platform_device_alloc" [/home/rdm/ethtest/eth-ins.ko] undefined! Do I need something to set in the Kernel Config? Helloworld works as LKM.

#include <linux/platform_device.h>#include <linux/module.h#include <linux/types.h>MODULE_LICENSE("GPL");MODULE_AUTHOR("Robert W. Oliver II");MODULE_DESCRIPTION("A simple example Linux module.");MODULE_VERSION("0.01");static struct platform_device *pd...

NKorn.3 by Associate
  • 1471 Views
  • 1 replies
  • 0 kudos

FDCAN not working properly

I am trying to enable FDCAN on STM32MP157C. I modified Linux Kernel (STM32MP15-Ecosystem-v2.0.0) and U-Boot, following the steps explained in the Developer Package guide. I get these messages, which are suggesting I setup everything correctly.root@st...

JYune by Associate II
  • 4350 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 MPUs Ecosytem Release V2.1 Distribution package not using device tree files from meta-st-stm32mp-addons.

I've been using Ecosystem v2.0 without any issues now. We decided to move to v2.1 recently, followed the instructions from https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package to get the latest package. Then, as I did before, followed the...

NBhat.1 by Associate III
  • 2077 Views
  • 3 replies
  • 0 kudos

STM32MP157A-DK1 update kernel

I Installed the Development on my host machine and builded a Kernel with this tutorial:https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txtbut afther the reboot my scren keeps beeing ...

SAman.1 by Associate III
  • 2747 Views
  • 5 replies
  • 0 kudos

Enable SPI5 on STM32MP157C-DK2 board

Hi everyone,I want to make a LoRa gateway using the STM32MP157C-DK2 and ICC880A-SPI boards. For that, I have to implement SPI communication between the two boards. I already did the hardware connections, but I am not able to enable SPI on the STM32MP...

LewisN by Associate
  • 1959 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.