‎2021-01-07 10:13 AM
Hello ,
New year 2021 Greetings:party_popper: ! Hope you all are doing great !
Looking at the FreeRTOS wiki , there is no support for Cortex - A7?
Is there an alternate port available for FreeRTOS for Cortex A7? or some customization for the same?
what is the recommendation?
Thanks and Regards,
Have a great Decade !!
D
Solved! Go to Solution.
‎2021-01-09 12:16 AM
Hello.
Tray to find RT-OS here CMSIS_5/CMSIS/RTOS2/Source at develop · ARM-software/CMSIS_5 (github.com)
Also, see my bare-metal project (without OS) running on A7 cores from 157-s: ua1arn/hftrx: Embedded firmware for ham radio transceivers (github.com)
STM32MP1 MPUs is a 32-bit processor.
I cant see cortex A7 in the link. - Cortex-A7 and A9 is a true compatible, Same interrupt handling, MMU and caches initialization,
Note: MMU is a required for enabling data cache write back feature,
‎2021-01-07 11:10 AM
Getting a complex SoC like STM32MP1 booted is a quite complex task. Especially if you think of Boot ROM, DRAM, clock tree, caches (?), virtual (?) memory setup, boot peripherals (sd-card ? usb ? network ?) including file systems (?) etc. Its much more than just porting the FreeRTOS core code to Cortex-A7. For the latter, see also http://www.freertos.org/Using-FreeRTOS-on-Cortex-A-Embedded-Processors.html
‎2021-01-08 8:43 AM
OK , so i read it as "no support". I cant see cortex A7 in the link.
Do you suggest any other alternative to this?
one question - is STM32MPU arm64 or arm32?
Regards,
‎2021-01-09 12:16 AM
Hello.
Tray to find RT-OS here CMSIS_5/CMSIS/RTOS2/Source at develop · ARM-software/CMSIS_5 (github.com)
Also, see my bare-metal project (without OS) running on A7 cores from 157-s: ua1arn/hftrx: Embedded firmware for ham radio transceivers (github.com)
STM32MP1 MPUs is a 32-bit processor.
I cant see cortex A7 in the link. - Cortex-A7 and A9 is a true compatible, Same interrupt handling, MMU and caches initialization,
Note: MMU is a required for enabling data cache write back feature,
‎2021-01-09 7:45 AM
> one question - is STM32MPU arm64 or arm32?
The answer is written literally in the FIRST line of the datasheet! And you know that it's a Cortex-A7 - it's ARM home page, Wikipedia and Google gives an answer in seconds...
As Genadi said - A7 and A9 are compatible and it should be relatively easy to port the code. But Knarf already warned on the complexity. Especially with such information finding skills...
‎2021-01-10 10:19 AM
thanks @Genadi Zawidowski​ i will have a look on this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.