2020-12-27 10:25 PM
Hello, ST Community
I have successfully implemented dB meter code on my STM32L4 Discovery kit and got SPL in dB,
But the code has .a file made by ST.
I want to implement dBSPL meter in STM32MP1 using PDM sensor. Can it support same .a file on MP1 board? Can I implement dBmeter on MP1?
Thanks,
Tarun
2021-01-11 5:03 AM
Hi @Tdhol.1 ,
Could you please share more details on the .a file ?
If this static library is L4 hardware dependent, the answer is no, otherwise I would say yes as both MP1 and L4 are 32bits ARM CPUs.
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.