STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I have a problem with the predictive maintenance setup as described in UM2639 and dm00659285..". I get as far as "Edge computing setup complete". Then it completely stops. Any ideas?

The handshake sequence looked a bit odd too. [STMdemo1] (08:07:40): {"state": {"reported": {"Device_Type": "STEVAL-IPD005V1", "Features": [], "Firmware": ""}}}Update request with token "40d4c70c-ec71-4946-9f7b-b6ad2719d965" acceptedI have also tried ...

PHarl.1 by Associate
  • 2423 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157 OTP voltage

Hi guys,I'm designing a custom board with STM32MP157C using the MB1263 board as reference.The MB1263 reference design shows the VDD_OTP pin tied to VDD, which is 3V3 for that particular board. My custom board uses VDD = 1V8 instead of 3V3. Should I t...

NCF by Associate II
  • 1588 Views
  • 1 replies
  • 0 kudos

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution Why?

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution...

Vlaty.1 by Senior
  • 1485 Views
  • 2 replies
  • 0 kudos

Resolved! change pin mux in TF-A build for i2c-bus i2c4

We would like to build the TF-A image with a different muxer settingfor i2c4. The usual setting is:i2c4_pins_a: i2c4-0 {   pins {      pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */      <STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */      bias-dis...

RGlie.1 by Associate II
  • 2026 Views
  • 2 replies
  • 0 kudos

Добрый день, �? решил одну проблему как подключить�?�? к stm32mp157a-dk1 по tcp

Good day, I solved one problem how to connect to stm32mp157a-dk1 over tcp. In the console, you need to write ifconfig eth0 192.168.1.5 ; net data-P ttyRPMSG0 ; net data-p8888 but I do not see data in the buffer ttyRPMSG0. in my program OpenAMP_TTY_ec...

Vlaty.1 by Senior
  • 1314 Views
  • 1 replies
  • 0 kudos

Resolved! gcc comand not found

Hello Everyone I wanted to Install Buildroot on my STM32MP157-DK2 according to this website:https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/Unfortunately as a beginner with OpenST-Linux and Yocto I got stuck at that ste...

Can't boot from SD card on STM32MP157A-EV1

I am trying to get this board up and running again after being away from it for a while, but I've been running into problems trying to boot from the SD card. I followed the instructions from the wiki here: https://wiki.st.com/stm32mpu/wiki/STM32MP15_...

CC by Associate II
  • 4057 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.