2024-10-09 11:22 PM
NOTE: Started PRServer with DBfile: /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, Address: 127.0.0.1:35035, PID: 9978
Loading cache: 100% | | ETA: --:--:--
Loaded 0 entries from dependency cache.
NOTE: /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb: ENABLE_PARTITIONS_IMAGE not enabled
Parsing recipes: 100% |##################################################################################################################################################| Time: 0:02:31
Parsing of 2868 .bb files complete (0 cached, 2868 parsed). 4596 targets, 530 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "2.4.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-24.04"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "stm32mp1"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "4.2.4-snapshot-20241010"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "mickledore"
ACCEPT_EULA_stm32mp1 = "1"
GCCVERSION = "12.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-networking
meta-webserver = "HEAD:aa5e8edabbc414d8ec1b2ad63c8743c7baf99626"
meta-st-stm32mp = "HEAD:1f152e07019dc06fd331b4926ec7e76ceae3d259"
meta-st-openstlinux = "HEAD:2636960b2bead3d1cb294e378e2b06ef8997189e"
meta = "HEAD:23b5141400b2c676c806df3308f023f7c04e34e0"
NOTE: Fetching uninative binary shim http://downloads.yoctoproject.org/releases/uninative/4.3/x86_64-nativesdk-libc-4.3.tar.xz;sha256sum=1c35f09a75c4096749bbe1e009df4e3968cde151424062cf4aa3ed89db22b030 (will check PREMIRRORS first)
WARNING: Your host glibc version (2.39) is newer than that in uninative (2.38). Disabling uninative so that sstate is not corrupted.
Initialising tasks: 100% |###############################################################################################################################################| Time: 0:00:11
Sstate summary: Wanted 3246 Local 0 Mirrors 0 Missed 3246 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
ERROR: PermissionError: [Errno 1] Operation not permitted
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
bb.utils.disable_network(uid, gid)
File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted
ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work) failed with exit code '1'
ERROR: PermissionError: [Errno 1] Operation not permitted
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
bb.utils.disable_network(uid, gid)
File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted
ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6 tasks of which 0 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 3 seconds
Summary: 2 tasks failed:
/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work
/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.
Solved! Go to Solution.
2024-10-11 12:02 AM
Hi,
as I said to you on another post, you need to move to Ubuntu 22.04 or 20.4.
Ubuntu 24 has not been tested.
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
Philippe.
2024-10-11 12:02 AM
Hi,
as I said to you on another post, you need to move to Ubuntu 22.04 or 20.4.
Ubuntu 24 has not been tested.
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
Philippe.
2024-10-11 12:08 AM - edited 2024-10-11 12:08 AM
i have moved to ubuntu 22.04 and i have downloaded distribution package but i cant find
FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv
2025-03-11 10:24 AM
Ok, so almost 6 months later and we still can't use Ubuntu 24? It is 2025.
Is this on this todo list?
2025-03-11 11:03 PM
yes u cant use ubuntu 24 as it has been tested with only ubuntu 22.04
2025-03-18 1:48 AM
Hi @Sharan
Please check the following wiki article which propose a solution for this issue: https://wiki.st.com/stm32mpu/wiki/System_build_troubleshooting_grid
BR
Jean-Philippe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.