2020-03-10 3:36 AM
Hi,
I am using STM32MP1 and setup STM32MP1_artificial_intelligence_expansion_packages to run AI algorithm.
Could you please guide me on: Is there any recommendation on which camera to use for AI application from ST side? Can I use Raspberry Pi camera or something like that with STM32MP1?
Thanking you,
Saurabh
Solved! Go to Solution.
2020-03-10 3:45 AM
Hi @SChau.2062
This will depend on the board you want to use. Please refer to material recommandation in wiki :
2.2 Material needed↑
To use the X-LINUX-AI-CV OpenSTLinux Expansion Package, choose one of the following materials:
Eg you can't connect a Raspberry Pi CSI camera on DK2.
Hope it help
Olivier
2020-03-10 3:45 AM
Hi @SChau.2062
This will depend on the board you want to use. Please refer to material recommandation in wiki :
2.2 Material needed↑
To use the X-LINUX-AI-CV OpenSTLinux Expansion Package, choose one of the following materials:
Eg you can't connect a Raspberry Pi CSI camera on DK2.
Hope it help
Olivier
2020-03-10 4:54 AM
Hi @Community member ,
Thanks for the detailed explanation.
Thanks,
Saurabh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.