2025-09-16 11:51 AM
Hi,
I have an STM32MP135F-DK board and I would like to know if to follow the steps in the video below I just need to install STM32CubeIDE on a computer running Linux or if I need to install something first?
https://www.youtube.com/watch?v=qEzfqKt3exE
For example, is it necessary to follow the steps corresponding to the links below first, or does the STM32CubeIDE installation itself and the sequence of steps in the video already do this?
Thanks,
Ari
2025-09-16 11:31 PM
Hello @AMend.7
You need to install the SDK for the MP1 before hand. It will be needed by CubeIDE to initialize OpenSTLinux components.
I recommend you to follow the getting started of the MP13 entirely if you haven't yet done it. It will allows you to have all the mandatory tools and sources to develop on Cortex A and M.
You can also refer to the Deep Dive section that is updated with recent version of OSTL and CubeMx (as the video is already 4y old).
Have a look at these category and pages I linked bellow
https://wiki.st.com/stm32mpu/wiki/Category:How_to
https://wiki.st.com/stm32mpu/wiki/Category:STM32CubeIDE
https://wiki.st.com/stm32mpu/wiki/How_to_install_the_Yocto_Project_SDK_in_STM32CubeIDE
https://wiki.st.com/stm32mpu/wiki/How_to_manage_STM32MP1_OpenSTLinux_projects_in_STM32CubeIDE
I hope this will help you!
Regards,
2025-09-19 10:25 AM
Hi, Pwxn
I followed the video to try to install OpenSTLinux using STM32CubeIDE for the STM32MP135F-DK board. However, in the current version, it is necessary to specify the installation directory, and when I choose a directory in HOME, the installation displays a dialog box informing me that it failed to install OpenSTlinux in the local folder.
Then I tried to install OpenSTlinux manually, as per the link below:
But I couldn't figure out which path to use in the commands below:
./stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sdk/st-image-weston-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.8-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.sh -d <absolute path to the working directory>/Developer-Package/SDK
Could you edit this command to include the path names as recommended?
2025-09-23 8:09 PM
Hello @AMend.7
If you follow the getting started you should recognize a pattern on how the packages are installed and where.
You can refer to this page to see ST' suggestion on structure :
https://wiki.st.com/stm32mpu/wiki/Example_of_directory_structure_for_Packages
I hope this help you.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.