STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RAM for STMP157

Hi,I am building my STMP157 board using the reference of "STMP15X-SOM" of Olimex. In that the RAM used is K4B4G1646D-BYK0, but I am unable to find the part number in online store. Can you please help me in finding the different RAM which can be used ...

muffss by Associate II
  • 2656 Views
  • 5 replies
  • 0 kudos

Size of the file read by ROM code

Hello,I am developing on the STM32MP131FAE board in a bare-metal environment.This chip does not have internal Flash, so I am planning to load a bin file from external Flash at initial boot.The Flash will store two bootloaders and two main firmware im...

Stnoobs by Associate II
  • 1153 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.