STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Many issues with STM32MP157F-DK2

1.) HAL_Delay(x) hangs forever when restarting CM4 using Hardware Timer for Systick. Every unit was forced with RESET/RELEASE. Any firmware change could not solve it. Have to repower the board. Happens in Normal and Engineering mode!2.) HAL_Init() ha...

Resolved! DCMIPP on STM32MP131

Looking at AN5478 implies that the entire line of STM32MP13x has a DCMIPP interface. However for STM32MP131 DCMIPP is not mentioned in the datasheet.Does the STM32MP131 have a DCMIPP interface? If so, are the pins and the functionality matching that ...

daikon by Associate
  • 1637 Views
  • 1 replies
  • 0 kudos

Resolved! cannot install build-essential pkg

I want to connect AWS IoT on STM32mp135f-dk board. so, I install pkgsudo apt-get install gitsudo apt-get install cmakesudo apt-get install build-essentialbut, can't auto install build-essential, so dpkg manual install.(build-essential_12.10_armhf.deb...

younghan by Associate III
  • 5816 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.