cancel
Showing results for 
Search instead for 
Did you mean: 

Use rotary encoder on stm32mp157

Jason007
Associate

 

I'm doing a project, that I need a rotary encoder working on cortex-a7 core of stm32mp157.

I met problem, my rotary encoder can not work. 

This is what I have done:

1. In kernel menuconfig I have config: use rotary encoder as a build-in module;

2. Write dts, and I am sure these gpio not been use anywhere:

    rotary@3 {
        compatible = "rotary-encoder";
        gpios = <&gpioa 0 GPIO_ACTIVE_LOW>, <&gpiog 3 GPIO_ACTIVE_LOW>;
        linux,axis = <6>;
        rotary-encoder,encoding = "gray";
        rotary-encoder,relative-axis;
        status = "okay";
    };
 
In dmesg I can see my roary is started
Jason007_1-1716992523494.png

In /proc/device-tree, I can see the device node

Jason007_1-1716992931386.png

In evtest nothing output, when I turn the knob of encoder.
Jason007_0-1716992396373.png

 

what is the problem, I need your help, thank you!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

HI @Jason007 

 

Did you have GPIOs pull-ups on the board ?

Maybe try if internal pull-up is ok by using

(GPIO_ACTIVE_LOW | GPIO_PULL_UP)

 

Alternatively (could reach higher count rate), you could use TIM or LPTIM for this (still need pull-ups).
See https://wiki.stmicroelectronics.cn/stm32mpu/wiki/How_to_use_the_IIO_user_space_interface#How_to_use_the_quadrature_encoder_with_the_sysfs_interface

(need to chose input pins according to Timers inputs possible muxing).

 

Regards,

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.