STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Mipi-dsi display problem

1,What is the reason for setting the display frequency to 50HZ instead of 60HZ?2, I designed a circuit board, using mipi to HDMI chip, and found that using 60HZ frequency to drive the display will jitter.

0690X000009jAoCQAU.png
Yli.8 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos

Reset MPU independently of MCU

Hello.I want to reset MPU core(s) while MCU is running firmware. Such reset shouldn't stop MCU.I can make electrical changes if it can be achieved with power control. Or maybe it can be possible to use PWR (or some other) registers?

alexey.b by Associate II
  • 1508 Views
  • 1 replies
  • 0 kudos

Resolved! sound alarm - stm32mp157c-dk2

I want to use sound alarm in my M4 program or on A7 Linux side.It can be any kind of sound (beep...etc).What should I do ?Which external pheriperal can I buy , or is it possible to do it with internal pheriperals on the board and how ?tnx

IYetk by Associate III
  • 1591 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.