2019-09-13 7:01 AM
I want to change resolution of display in ev kit but don't know how to do.
Should I change the default struct values in panel-raydium-rm68200.c or is there another method?
Also, I'd like to rotate the screen of TFT so it will be wide screen TFT, is it possible? (For in compile time not run time)
Finally, need to add a custom TFT instead of this. Which parameters do I need to add a new one?
2019-09-16 5:17 AM
Hi @gokhannsahin
Display settings are defined in [output] section of the weston.ini file.
https://wiki.st.com/stm32mpu/wiki/Wayland_Weston_overview
Please refer also to weston documentation here
http://manpages.ubuntu.com/manpages/disco/en/man5/weston.ini.5.html
Resolution have to be manage in "mode" option, rotation with "transform" option
To add a new custom TFT, depending on the used interface, you might deal with drivers and Device Tree configuration.
Olivier
2019-09-16 5:24 AM
Hi,
You can find detailed tutorial to change display mode in this article
https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI#Video_modes
Hope it help
Olivier
2019-09-21 6:29 AM
Thank you @Community member
I'm using openstlinux-eglfs distro, is it valid for openstlinux-eglfs too?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.