Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Board: STM32MP157A-DK1Situation: I have the release 2.6-openstlinux-4.19-thud-mp1-19-02-20 on the A7 core running. I created a simple FreeRTOS LED app with the latest CubeMX for the M4 core. The FreeRTOS interface ist CMSIS V2. The SYS Timebase Sourc...
I compiled uboot and Linux kernel packages, used a brand new SD card.and used "sgdisk" to divide them into five areas. fsbl1,fsbl2,ssbl,bootfs,rootfs.Use the following command to complete the burning of u-boot:---------------------------------------...
I have problems with different SDIO WiFi Modules on the stm32mp157-dk2. Those Modules are connected to the sdmmc3. The modules are qca9377-3 and wilc3000. Both Modules are slow compared to the on the dk2 embedded device and both are slow compared to ...
We designed our own board and use RTL8211E instead of RTL8211EG-VB-CG. We are unable to get the PHY device to respond although we copy the same circuit from the MB1262. The MAC is working but the communication to Realtek PHY seems to be a problem. ...
According to the documentation of the EV1 eval board:"The STM32MP157xAA3 also drives a sub system reset, SUB_NRST signal on PD10 IO, to the peripherals: USB Host Hub, MFX, Ethernet, and RGB_LTDC connector."Is this signal generated automatically by th...
Hi,I am building openstlinux-weston/st-image-weston image for stm32mp157c-dk2 board, and I have developed 2 application to be displayed at the same time. I configured DSI and HDMI with Buildroot, for the last one I followed this wiki: https://wiki.st...
Hello all,I am trying to use the SPEAKER_OUT connector in the STM32MP157C-EV1 board to play sound using a set of regular 8 Ohm (non-amplified / passive) loudspeakers.I am configuring the wm8994 to enable the SPKOUTL/RP path as described here: https:/...
Hey all,I have a STM32MP157C-DK2 developer board with screen and i am trying to get node.js running on it. Has anyone done this before? I know the board is pretty new, released in Oktober. But worth a shot.ThanksRinke
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.