STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm trying to find a solution to a problem using vision with ANN/CNN - STM32Cube.AI or X-LINUX-AI-CV or FP-AI-VISION1 or X-CUBE-AI

I'm trying to find a solution to a problem using vision, I discovered the 'MPU' line with the STM32MP157C-DK2 but while investigating I cannot find CSI input or even a camera input. While I enjoy playing with USB based cameras it is 2019 and everyone...

KevinA by Senior
  • 2199 Views
  • 5 replies
  • 0 kudos

opengl no wayland

Is it possible to use opengl without wayland?the /vendor/lib libraries have dependency to libwaylandand as far as i am aware these libraries are binary only.are there other versions of the libraries that can work with fb, without x or wayland?otherwi...

Resolved! board_check_usb_power issues on EV1

Hello,After power on my EV1 board, I get the following error message:NOTICE: CPU: STM32MP157AAA Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother NOTICE: Board: MB1263 Var1 Rev.C-01 INFO: Reset reason (0x15): INFO...

BryanWang by Associate II
  • 1859 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.