STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I configure additional rootfs(additional Directory, more Package like as lighttpd)?

Hello everyone.​I am modifying the distribution packages of 157C-DK2 and 157C-EV1 for my project.​When I previously configured my rootfs using buildroot and debian-jessie, I proceeded as follows(other boards).Packages that can be configured using bui...

0693W000003PiZCQA0.png
SPark.15 by Associate II
  • 4272 Views
  • 4 replies
  • 0 kudos

How to compile device tree for board ODYSSEY-STM32MP157C on arm-ostl-linux-gnueabi/linux-stm32mp-5.4.31-r0

Hi,I'm using your wikihttps://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernelto add some device threes that belongs to a different board ...

Resolved! STPMIC1 efficiency at low load

Dear all, I am looking to use the STPMIC1 in one new STM32MP15x design which will spend most of this time in standby mode. I am looking for STPMIC1 buck efficiency at light load (~1mA). In the datasheet there is numbers only for 150mA, 750mA and 1A. ...

PGE by Associate III
  • 2367 Views
  • 2 replies
  • 0 kudos

Boot to v5.4-stm32mp-r1

Hello,has anyone successful booted linux  v5.4-stm32mp-r1 on the stm32mp157c-dk2 board?If so can you please provide me a working config?I am trying to switch from the 4.19 kernel to v5.4-stm32mp-r1 but the boards freezes after trying to load the kern...

Artem by Associate III
  • 3584 Views
  • 5 replies
  • 0 kudos

Hello, I have a question regarding ST marketing on the STM32MP1 devices. According to the page, it states "STM32MP1 users can now choose from several IDEs from leading vendors and enjoy free license"

Which IDEs can be used for free in order to download/debug my application in an asynchronous fashion as two cores are running the the same time. I have taken a look on some suppliers (Tools & Software), but it looks like that you need to pay a some m...

PBart.3 by Associate II
  • 6435 Views
  • 10 replies
  • 1 kudos

Power startup with discrete power supply

Dear All,According to AN5256 "discrete power supply hardware integration" the power source for VDD is turned off in case of crash to "reset" the hardware using the PWR_ONRST signal. At startup. At cold startup and immediately after a crash the power ...

PGE by Associate III
  • 1290 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.