2020-08-09 3:11 PM
Hello,
has anyone successful booted linux v5.4-stm32mp-r1 on the stm32mp157c-dk2 board?
If so can you please provide me a working config?
I am trying to switch from the 4.19 kernel to v5.4-stm32mp-r1 but the boards freezes after trying to load the kernel without any output, until it gets restarted by the WDG.
I have tried to use TF-A and also U-Boot as SPL, both with the same results.
Kernel 4.19 and also stock 5.7 are booting just fine... The kernel configs are also the same.
U-Boot SPL 2020.01-stm32mp-r1 (Aug 09 2020 - 23:04:31 +0200)
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
RAM: DDR3-DDR3L 16bits 533000Khz
WDT: Started with servicing (32s timeout)
Trying to boot from MMC1
U-Boot 2020.01-stm32mp-r1 (Aug 09 2020 - 23:04:31 +0200)
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in basic mode (st,stm32mp157c-dk2)
Board: MB1272 Var2.0 Rev.C-01
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
In: serial
Out: serial
Err: serial
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
Boot over mmc0!
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Found /boot/extlinux/extlinux.conf
Retrieving file: /boot/extlinux/extlinux.conf
131 bytes read in 35 ms (2.9 KiB/s)
1: stm32mp157c-dk2-buildroot
Retrieving file: /boot/zImage
3986960 bytes read in 203 ms (18.7 MiB/s)
append: root=/dev/mmcblk0p4 rootwait
Retrieving file: /boot/stm32mp157c-dk2.dtb
105200 bytes read in 40 ms (2.5 MiB/s)
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
Loading Device Tree to cffe3000, end cffffaef ... OK
Starting kernel ...
2020-08-09 9:50 PM
Hi,
had the same problem as well:
For me using the .config file of the released kernel (not the one on the ST Github, I am talking about the on eyou can get here: https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Downloading_the_Linux_kernel) fixed the problem.
Hope it helps.
2020-08-10 1:06 AM
Hello,
ok, now I have also extracted the config from the "released" kernel, but it still not boot. Have you applied any patches?
2020-08-10 1:21 AM
Yes i applied the config fragments according to the README (till including step 5).
2020-08-10 2:32 AM
Ok, I got it working now:
I have extracted and patched the kernel like explained in the README. Then I have generated the config with all fragments - also like explained in the README (till fragment 5 too). Now I have copied over the full config to buildroot and was able to compile the v5.4-stm32mp-r1 kernel from github.
The kernel now boots when using TF-A but not U-Boot SPL, but this is fine for me.
It would be good to know what piece of config is preventing the kernel from booting...
2020-08-24 6:15 AM
Hi @Artem
>> The kernel now boots when using TF-A but not U-Boot SPL, but this is fine for me.
This is inline with the ecosystem release V2.0 in which support of basic boot chain ( start kernel from U-Boot SPL ) has been removed.
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.