2020-08-20 6:25 AM
Dear all,
I am looking to use the STPMIC1 in one new STM32MP15x design which will spend most of this time in standby mode.
I am looking for STPMIC1 buck efficiency at light load (~1mA). In the datasheet there is numbers only for 150mA, 750mA and 1A. Is there any additonal numbers or graphics available somewhere ? I can see there is a special LP mode for light load but there is no indication about efficiency in LP mode.
Many thanks in advance for your help
Solved! Go to Solution.
2020-08-24 5:54 AM
Hi @PGE
Did you notice Figure 3 to Figure 6 in DS ?
They contains efficiency for bucks in all range from 0.0001A to 1A in both HP and LP mode.
Isn't it what you are looking for ?
Olivier
2020-08-24 5:54 AM
Hi @PGE
Did you notice Figure 3 to Figure 6 in DS ?
They contains efficiency for bucks in all range from 0.0001A to 1A in both HP and LP mode.
Isn't it what you are looking for ?
Olivier
2020-08-24 6:41 AM
Yes thanks ! I don't know why I didn't notice them...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.