2020-08-26 5:14 AM
I am designing a board using STM32MP1, STPMIC1A and LPDDR2. I want to use 3.3V VDD not 1.8V as most of peripherals are 3.3V. I am following example in AN5031 Figure 32 LPDDR2 VDD1 is powered from LDO3 in bypass mode which is powered by VDD 1.8V.
I plan to change BUCK3 settings to output VDD 3.3V, use BUCK 4 to output 1.8V to power LDO3 in bypass mode which power LPDDR2 VDD1. I can't use BUCK directly to power LPDDR2 VDD1 as BUCK4 is rank 2 and turn on automatically with default 3.3V.
Is that the correct/recommended way to do it ?
Thanks in advance
Solved! Go to Solution.
2020-08-28 2:15 AM
Hi @PGE
Actually you can generate the 1.8V from LDO3 using normal mode and any input between 2.8V to 5.5V. ( eg 3.3 from BUCK3)
You suggestion using BUCK4 as pre-regulation to 1.8V + LDO bypass is also possible and you will gain a bit on efficiency/power consumption. ( if this is important for you)
With STPMIC1A BUCK3 is already at 3.3V by default so you don't have to change anything.
Hope it help,
Olivier
2020-08-28 2:15 AM
Hi @PGE
Actually you can generate the 1.8V from LDO3 using normal mode and any input between 2.8V to 5.5V. ( eg 3.3 from BUCK3)
You suggestion using BUCK4 as pre-regulation to 1.8V + LDO bypass is also possible and you will gain a bit on efficiency/power consumption. ( if this is important for you)
With STPMIC1A BUCK3 is already at 3.3V by default so you don't have to change anything.
Hope it help,
Olivier
2020-08-28 2:46 AM
Thanks for the reply. Yes power consumption/efficiency is important for me (hence the LPDDR2 choice). Will use BUCK3 in 1.8V mode.
Thanks again
2020-08-28 5:26 AM
Hi @PGE
BUCK3 ? Guess you mean BUCK4 in 1.8V right ? :smiling_face_with_smiling_eyes:
Olivier
2020-08-28 6:28 AM
Yes right BUCK4 sorry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.