2020-08-24 6:40 PM
Hi,
I want to update the boot chain (basic mode) for a "custom" device tree.
Following the wiki page below, I understood how to update the boot chain (trusted mode) for a "custom" device tree.
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
On the other hand, I don't know how to update the boot chain (basic mode) for a "custom" device tree.
In basic mode, should I compile the device trees in the following steps?
==U-boot==
make stm32mp15_basic_defconfig
make DEVICE_TREE=<device tree> all
==TF-A==
make -f ../../sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.0-r0/Makefile.sdk TFA_DEVICETREE=<device tree> TF_A_CONFIG=basic all
In this case, which files should I copy into the 'fsbl1', 'fsbl2' and 'ssbl' partition of the target?
Best Regards.
H. Masuda
Solved! Go to Solution.
2020-08-28 1:56 AM
if it helps, i using GDB debugger that came with STM32CubeIDE to debug m4 firmware with linux and with IS_ENGINEERING_BOOT_MODE you can search for this option on st wiki . works grate .
2020-08-25 1:08 AM
Hi @HMasu.1
Seems you made some confusion regarding what is "basic" boot.
Please refer to https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Boot_chains_overview ( archived wiki aligned with V1 ecosystem delivery ) to clarify difference between so called "trusted" and "basic" boot chain.
Anyway "basic" boot chain was already not recommended in ecosystem V1 and is now deprecated/removed in ecosystem V2.
ST will not provide any further support for it.
We fully recommend to switch to Trusted boot chain.
Olivier
2020-08-26 4:51 PM
Hi @Community member
Thank you for your answer.
I read the page you taught me, and I have understood that the basic boot chain is only provided to support the DDR Tuning Tool and the U-Boot developments.
On the other hand, I was explained by Real Time OS vendor that I need to use "basic" boot chain when I want to attach MDK-ARM(ULINK) debugger to Cortex-M4.
I want to use "basic" boot chain for above reason.
Does it mean that the basic boot chain is not supported/promoted to make products, but I can use only for debugging?
Or, is the explanation of Real Time OS vendor wrong?
Best Regards.
H. Masuda
2020-08-28 1:47 AM
Hi @HMasu.1
Can you point me resource from your Real Time OS vendor about this topic.
I don't see obvious relation between M4 debugger attachment and Linux boot scheme.
Olivier
2020-08-28 1:56 AM
if it helps, i using GDB debugger that came with STM32CubeIDE to debug m4 firmware with linux and with IS_ENGINEERING_BOOT_MODE you can search for this option on st wiki . works grate .
2020-08-30 6:14 PM
Hi @Community member (ST Employee)
Thank you for your answer.
I was explained by e-mail from Real Time OS vendor that, by using "trusted" boot chain , ARM Trusted Firmware seems to block the ports required for JTAG access, so I need to use "basic" boot chain when I want to attach MDK-ARM(ULINK) debugger to Cortex-M4.
Is the explanation of Real Time OS vendor wrong?
In any case, I will use "trusted" boot chain because I have understood that ST recommend to switch to Trusted boot chain.
Best Regards.
H. Masuda
2020-08-30 6:20 PM
Hi @SMich.1
Thank you for your valuable information.
I will search STM32CubeIDE GDB debugger option on ST Wiki.
Thank you.
H. Masuda
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.