STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have compiled the stm32mp157 disco V2.0.0.0 Distribution package for both the x11 (matchbox desktop) and the x11-xfce image, insuring that I accept the EULA. When I run both images, response times and memory image are very large compared to V1.2

I have xfce running very well in the V1.2 Yocto Distribution system on the stm32mp157c disco board. The xfce desktop is very responsive and uses about 100M of memory. The xfce desktop using the latest V2.0.0 Distribution image however is very sluggi...

STild.1 by Associate
  • 2459 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157AAA can not boot

Hello,PLEASE GIVE SOME HELP.We made some boards based on MP157AAA and it ran good at first.BUT it can not boot anymore after someone turn off and on the power.No information comes from UART4 after turn on power switch.I change the boot-switch to '00...

0693W000004KLOFQA4.png 0693W000004KLTFQA4.png
Ssun.21 by Associate
  • 1832 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.