STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Am I the first one trying to run openstlinux-eglfs/st-example-image-qt on stm32mp157c-dk2?

Hi Folks,I am trying to build openstlinux-eglfs/st-example-image-qt using yocto/openstlinux distribution (please see details below) for stm32mp157c-dk2 board. After fixing compilation problem with qt3d (scene2d example failed to compile) I was able t...

AndreyN by Associate III
  • 10413 Views
  • 5 replies
  • 0 kudos

STM32MP153/157 periphery

Hey,As a hardware engineer, I worked for a long time with the M7 controller.For a Specific Algorithm, It seems like I should use a stronger core then the M7 480Mhz, when the purpose is to Calculate in Real-time.one of the options is to use the MP153/...

Pkats.1 by Associate II
  • 1979 Views
  • 1 replies
  • 0 kudos

Resolved! How to use remoteproc on STM32MP151?

I want to use remoteproc to load and start firmware on Coretex-M4 from Cortex-A7.I refer to the following Wiki page.https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overviewIn above Wiki page, I have tried [4.1.1 Remote processor boot thr...

HMasu.1 by Senior
  • 7853 Views
  • 18 replies
  • 0 kudos

Resolved! How to get STM32Cube_FW_MP1_V1.2.0RC2?

want to exchange large data buffers with the coprocessor.I have done following wiki page.​https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example#Source_code​I want to analyze Cortex-M4 source ...

HMasu.1 by Senior
  • 1386 Views
  • 2 replies
  • 0 kudos

Resolved! Is there any sample source code that implements the transfer from Cortex-A to Cortex-M?

I want to implement the program that exchange large data with each other on Cortex-A7 and Cortex-M4 by using DDR.​Thanks to following wiki page, I have understand the mechanism that exchange large data from Cortex-M4 to Cortex-A7 by using DDR.​https...

HMasu.1 by Senior
  • 3629 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.