2020-10-25 2:04 AM
The handshake sequence looked a bit odd too.
[STMdemo1] (08:07:40): {"state": {"reported": {"Device_Type": "STEVAL-IPD005V1", "Features": [], "Firmware": ""}}}
Update request with token "40d4c70c-ec71-4946-9f7b-b6ad2719d965" accepted
I have also tried a manual boot using /home/root/start_pmp.sh where it gets one step further with "Demo running..." then stops.
Any help appreciated. Phil
Solved! Go to Solution.
2020-10-27 10:37 AM
Hello Phil,
yes, you are right, the handshake sequence is missing the features and the firmware version; it should look, for example, like this:
[<device>] (<timestamp>): {"state": {"reported": {"Device_Type": "STEVAL-IPD005V1", "Features": ["Environmental", "Inertial_TDM", "Inertial_FDM"], "Firmware": "Firmware Ver.1"}}}
Have you tried to compare the output log to the log reported in Chapter 4.1 of the manual? Can you post it here, please?
Moreover, have you tried to flash again the firmware of the sensor devices and the master board?
Regards,
Davide
2020-10-27 10:37 AM
Hello Phil,
yes, you are right, the handshake sequence is missing the features and the firmware version; it should look, for example, like this:
[<device>] (<timestamp>): {"state": {"reported": {"Device_Type": "STEVAL-IPD005V1", "Features": ["Environmental", "Inertial_TDM", "Inertial_FDM"], "Firmware": "Firmware Ver.1"}}}
Have you tried to compare the output log to the log reported in Chapter 4.1 of the manual? Can you post it here, please?
Moreover, have you tried to flash again the firmware of the sensor devices and the master board?
Regards,
Davide
2020-10-28 6:37 AM
2020-10-29 2:38 AM
You are welcome, Phil.
Regards,
Davide
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.