2020-11-30 7:06 AM
#include <linux/platform_device.h>
#include <linux/module.h
#include <linux/types.h>
MODULE_LICENSE("GPL");
MODULE_AUTHOR("Robert W. Oliver II");
MODULE_DESCRIPTION("A simple example Linux module.");
MODULE_VERSION("0.01");
static struct platform_device *pdev;
static int __init fake_eth_add(void)
{
int inst_id = 0;
pdev = platform_device_alloc("fake-eth", inst_id);
return 0;
}
static void __exit fake_eth_put(void)
{
}
module_init(fake_eth_add);
module_exit(fake_eth_put);
2020-12-02 2:40 AM
Hi @Community member
Did you refer to following wiki page ?
Such kind of error usually come from bad installation / initialization of the SDK.
Double check your environment.
Hope it help,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.