2020-11-29 7:17 AM
HI,all,
env:virtualbox, ubuntu18.04 64bits, 10G memory,500G disk.
I tried to build rootfs image from stm32 Yocto prject, followed by wiki(https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package).
but I got some error at last like below.
I am a newer for YOCTO, what can I do next? any idea?
Thanks a lot.
error log:
ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs.11363
ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs) failed with exit code '1'
2020-11-30 6:30 AM
Hi @LKevi.1 ,
Did you have this error after executing bitbake st-image-weston ?
Could you please share the logfile of failure (log.do_rootfs.11363) ?
BR,
Christophe
2020-11-30 7:10 AM
Hi, Christophe Guibout:
Yes, I got this error after executing bitbake st-image-weston, like below log, and the detail log as attach
Thanks for your reply!
$ bitbake st-image-weston
NOTE: Started PRServer with DBfile: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 36013, PID: 21361
Loading cache: 100% |###########################################################################################| Time: 0:00:03
Loaded 3743 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.46.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "stm32mp1"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "3.1-snapshot-20201130"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "dunfell"
ACCEPT_EULA_stm32mp1 = "1"
GCCVERSION = "9.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-python
meta-oe
meta-gnome
meta-initramfs
meta-multimedia
meta-networking
meta-webserver
meta-filesystems
meta-perl = "HEAD:144077083457ccb75700777d5e6b1da9aaff01aa"
meta-st-stm32mp = "HEAD:955b1d9a5f706013d718687b1afa6e3022c68fac"
meta-qt5 = "HEAD:fdd19517e17240b0b61765bd02fc483a1bde986f"
meta-st-openstlinux = "HEAD:9160c08dfcd0b7ec0eb8f1fd96672695b09680d5"
meta = "HEAD:b39bda4cc62db12c0edfbe489d5a7f5988ede6a9"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:14
Sstate summary: Wanted 415 Found 398 Missed 17 Current 2904 (95% match, 99% complete)
NOTE: Executing Tasks
ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs.21480
ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs) failed with exit code '1'
Waiting for 3 running tasks to finish:
ERROR: st-image-userfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_immodules_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs.21635
ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb:do_rootfs) failed with exit code '1'
ERROR: st-image-weston-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_immodules_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-weston/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-weston/1.0-r0/temp/log.do_rootfs.21723
ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb:do_rootfs) failed with exit code '1'
ERROR: st-image-vendorfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs.21645
ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb:do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 9046 tasks of which 9031 didn't need to be rerun and 4 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 20 seconds
Summary: 4 tasks failed:
/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs
/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb:do_rootfs
/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb:do_rootfs
/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb:do_rootfs
Summary: There were 4 ERROR messages shown, returning a non-zero exit code.
2020-12-01 9:28 AM
HI @LKevi.1 ,
Unfortunately, the logs don't give more information.
I would recommand to restart the compilation : bitbake st-image-weston -c cleansstate && bitbake st-image-weston
If it still doesn't work, you can cleanup a bit more : bitbake st-image-weston -c cleanall && bitbake st-image-weston
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.