2020-11-25 3:42 AM
I am trying to enable FDCAN on STM32MP157C. I modified Linux Kernel (STM32MP15-Ecosystem-v2.0.0) and U-Boot, following the steps explained in the Developer Package guide. I get these messages, which are suggesting I setup everything correctly.
root@stm32mp1:~# dmesg | grep m_can
[ 3.032730] m_can_platform 4400e000.can: m_can device registered (irq=51, version=32)
[ 44.537911] m_can_platform 4400e000.can can0: bitrate error 0.3%
[ 44.542503] m_can_platform 4400e000.can can0: bitrate error 0.3%root@stm32mp1:/sys/kernel/debug/pinctrl/soc:pin-controller@50002000# cat pinconf-pins | grep CAN
pin 11 (PA11): alternate 9 (FDCAN1_RX) - push pull - floating - low speed
pin 12 (PA12): alternate 9 (FDCAN1_TX) - push pull - floating - low speedThe board seems to pass the internal loopback test as well (https://wiki.st.com/stm32mpu/wiki/How_to_send_or_receive_CAN_data#Hardware_self-test).
The problem is that I cannot get anything on the physical ports. What could have gone wrong?
2020-11-25 3:48 AM
Hi @JYune
We have a known bug with CAN we have already identified and pending to integrate :
You can find a version of patch here : https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/commit/?id=b0342b87cad88894a989604df549e88ff47fb513
Olivier
2020-11-30 10:12 PM
Hi Olivier,
I'm having the exact same problem as described in this issue. I'm testing FDCAN on our custom board based on STM32MP153C using Ecosystem v2.1.0 . Internal CAN loopback works fine but nothing on the physical pins. I also tried the kernel patch you suggested above but it didn't make any difference. I've also removed the "sleep" mode for the CAN pins and from m_can1 node from the kernel DT, but still no data on FDCAN1_TX pin when I try sending some data out. Am I missing something? Thanks.
2020-12-01 1:40 AM
@NBhat.1 I disabled loopback and was able to get physical signals.
2020-12-01 9:37 AM
Thanks @JYune I got it working with the above patch.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.