2020-11-29 9:35 PM
I've been using Ecosystem v2.0 without any issues now. We decided to move to v2.1 recently, followed the instructions from https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package to get the latest package. Then, as I did before, followed the instructions from https://wiki.st.com/stm32mpu/index.php/How_to_create_your_own_machine to create the distribution for our custom board. But running bitbake-st-image-weston failed because it could not create project.dtb as the project.dts files were not copied from the meta-st-stm32mp-addons folder to their respective folders in tf-a, u-boot and kernel.
Has anything changed in v2.1 with regards to custom device tree file placement?
Solved! Go to Solution.
2020-11-30 10:16 PM
This issue is now fixed.
Root cause: In Ecosystem v2.0 ENABLE_CUBEMX_DTB ?= "1" was set in the cubemx-stm32mp.bbclass, but in ecosystem v2.1 this macro is supposed to be set in machine.conf file. It is set to 0 in cubemx-stm32mp.bbclass.
2020-11-29 9:48 PM
I also noticed that when I ran this command
$> MACHINE=stm32mp1-<ProjectName> DISTRO=openstlinux-weston source layers/meta-st/script/envsetup.sh
It didn't give me an option to agree to EULA certificate and printed the following (with ecosystem 2.0 it sued to give an option to accept EULA and WITH_EULA_ACCEPTED said Yes)
Configuration files have been created for the following configuration:
DISTRO : openstlinux-weston
DISTRO_CODENAME : dunfell
MACHINE : stm32mp1-midmark
BB_NUMBER_THREADS : <no-custom-config-set>
PARALLEL_MAKE : <no-custom-config-set>
BUILDDIR : build-openstlinuxweston-stm32mp1-midmark
DOWNLOAD_DIR : <disable>
SSTATE_DIR : <disable>
SOURCE_MIRROR_URL : <no-custom-config-set>
SSTATE_MIRRORS : <disable>
WITH_EULA_ACCEPTED: <no-custom-config-set>
2020-11-30 7:57 AM
I upgraded my system to from ubuntu 16.04 LTS 18.04 LTS (as required by ecosystem v2.1) and restarted the whole process of distribution package. Now I do get EULA acceptance pop-up, but still the build fails because the custom device tree files from the addons are not linked in tf-a, u-boot and kernel source folders.
2020-11-30 10:16 PM
This issue is now fixed.
Root cause: In Ecosystem v2.0 ENABLE_CUBEMX_DTB ?= "1" was set in the cubemx-stm32mp.bbclass, but in ecosystem v2.1 this macro is supposed to be set in machine.conf file. It is set to 0 in cubemx-stm32mp.bbclass.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.