STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Linux RT patch on STM32MP157F

Hi, CommunityI'm building linux based firmware on STM32MP157F ad I need to apply linux RT patches.I'm using STM32MP157F-EV1 for testingAs linuxkernel I'm using ST linux v5.10-stm32mp-r2, of STMicroelectronics linux repo. This tag is v5.10.61 kernel v...

axel101 by Associate III
  • 1958 Views
  • 1 replies
  • 0 kudos

our stm32mp157F based custom board will not boot up, we see the panic error message on the uart interface.

hi,we are trying to flash our yocto build on our custom board using the stm32cubeprogrammer via usb in dfu mode. the flashing fails w/ the following message:19:33:39 : Opening and parsing file: tf-a-stm32mp157f-nff-mx-usb.stm3219:33:39 :  File      ...

vbuon.1 by Associate III
  • 2011 Views
  • 2 replies
  • 0 kudos

LAN8720 Device Tree changes

HI all,We are using LAN8720 as the ethernet PHY for connectivity.The IC has 25MHz crystal connected for the refclk and we want to run in RMII mode. We have requirement of not using the INT_N for the ethernet IC.Upon exploring the ST Docs I was not ab...

NPal.2 by Senior
  • 1814 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.