2022-01-26 10:30 PM
Hi ,
We are using the STM32MP157-dk1 board. We are able to boot the both cores (cortex A7) bare metal code from the SRAM but where as loading to the DDR that time only core 0 is booting properly and core 1 not booting. Is their any way to enable the DDR accessing to core1(second A7).
2022-01-26 11:17 PM
Hi,
As far as I know, there is no specific setting related to core1. Maybe the default MMU setting avoid it (for security purposes, BootROM likely strongly limit Cortex-A access regions during boot).
I will check with expert.
Did you start second core as listed in https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Secondary_core_boot ?
I think you should try starting second core with BRANCH_ADDRESS pointing internal SYSRAM code (e.g. to check if core#1 really start but also to allows, if needed, to setup correctly the second core MMU before accessing DDR).
Regards.
2022-01-26 11:27 PM
Thank you for the reply. I am following the below procedure, by this second core is running properly .
2022-01-27 12:48 AM
Thank you for the reply. I am following the below procedure, by this second core is running properly .
2022-01-27 3:11 AM
Hi,
I got confirmation from expert that the BootROM allows BRANCH_ADDRESS to DDR range.
Maybe some clues
Regards.
2022-01-31 1:04 AM
Hi,
I had tried in SRAM both the cores are working fine . When i am placing the code in DDR , when i am trying to run the code in situation core 1 is working fine but core 2 is not triggering. for this what may be the region.
2022-01-31 11:43 PM
Hi, I see no specific HW settings which should avoid 2nd core to access DDR.
Maybe have a look on how uBoot is starting 2nd core, e.g. https://github.com/ni/u-boot/blob/master/arch/arm/mach-stm32mp/psci.c#L119
You might need to debug/trace the 2nd core.
If the start or 2nd core in SYSRAM is ok, maybe check from this point if access/jump from SYSRAM to DDR is possible.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.