STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong? Sincerely, Alexander.

Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong?Sincerely, Alexander. ////////////////////////////////...

Vlaty.1 by Senior
  • 1694 Views
  • 2 replies
  • 0 kudos

Realtek RTL8211 alternatives?

Hello there,We are working on a design based on the STM32MP1 eval kit which is using Realtek RTL8211 for Ethernet.However this IC seems to be hard to buy; Realtek distributors are giving lead times of +1 year.Can someone recommend alternatives?Thanks...

Panic during custom board bring-up

We are trying to bring-up our custom board and every step of the way we see panic messages, we need some direction in understanding what went wrong. Our board has the following:Processor: STM32MP157FACxQSPI NAND flash memory is our boot device (AS5F1...

SKris by Associate III
  • 3372 Views
  • 2 replies
  • 0 kudos

Resolved! Steps to Lowest power

From my understanding of the documentation, my steps to lowest power (VBAT mode) on the STM32MP1-DK2 kit would be: Connect Battery to VBATSet BREN in TF-ADisable wake sources other than from PMIC and RTCenter sleep via: "echo mem > /sys/power/state"I...

BBeck.1 by Associate II
  • 8474 Views
  • 11 replies
  • 0 kudos

Resolved! STM32MP1 ecosystem 3.10 Developer package kernel fails to build on Ubuntu 21.10 (glibc 3.22 not found)

make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 GEN    Makefile HOSTCC scripts/mod/mk_elfconfig/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/ld: /usr/lib/gcc/x86_64-linux-gnu/11/libl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.