STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Pinout/Functionality between STM32MP1 devices and development boards, are they mostly similar?

Hello,I would like to embark on a project for a custom board with the STM32MP157DAB1 and I am referencing the STM32MP15-DISCO schematic from ST which uses the STM32MP157CAC3.My Question: How do I translate between the functionality of the pins?From o...

0693W00000Hqit7QAB.png
daded.1 by Associate II
  • 2848 Views
  • 3 replies
  • 0 kudos

Resolved! LAN8720 Custom SOM Issue

We have custom SOM which has been designed with STM32MP157C.We are using the OpenSTLinux 3.0.0 as of now as the distribution running on it.In case of LAN PHY interfacing we are using LAN8720.There is a strange behavior , upon I can see the below mess...

0693W00000Hr4uWQAR.png
NPal.2 by Senior
  • 2112 Views
  • 3 replies
  • 0 kudos

Resolved! ADC sampling from ANA0/ANA1 via M4

Hi,I have some doubts about how I could sample from the ANA0/ANA1 pins of an STM32MP1 CPU from inside the M4 firmware via HAL. I would like to programmatically switch between these two pins.Sampling from ADC_CHANNEL_0 seems to work, so I guess it is ...

ATringali by Associate II
  • 2888 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.