2022-01-24 1:41 AM
HI all,
We are using LAN8720 as the ethernet PHY for connectivity.
The IC has 25MHz crystal connected for the refclk and we want to run in RMII mode.
We have requirement of not using the INT_N for the ethernet IC.
Upon exploring the ST Docs I was not able to figure out the same.
What should be the correct device tree configuration for the same? We need to get it up correctly for each of TF-A , U-BOOT and Kernel ? So looking for answer around the same for device tree changes for each of these.
LAN8720 + RMII Mode + REFCLK with no using the INT_N interface.
Really appreciate the help.
2022-02-01 6:37 AM
Hi,
Sound like this would be ok for you :https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#RMII_with_Crystal_on_PHY_-28Reference_clock_-28standard_RMII_clock_name-29_is_provided_by_a_Phy_Crystal-29
For PHY_INITN pin, if not used, just forget it in the pinmux node (we don't use it on our boards, even if present on the HW).
Maybe some more info in AN5031.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.