2023-07-10 1:15 AM
Hello. We already have a custom board based on STM32MP151CAD3 with an eMMC. The following pins are different with default eMMC pins.
SDMMC2_CMD: PA0
SDMMC2_D1: PB7
As not default pins are used, we need to update OTP value. Here are my result.
OTP3 = 0x00000004
emmc_if_id=2: SDMMC2(uses non default AFmux defined in OTP).
OTP5 = 0x27A41094
SDMMC2_CMD = PA0 (bits[15:0]: port0=1=GPIOA, pin0=0, afmux0=9, mode0=4=AF;pull-up;medium-speed)
SDMMC2_D1 = PB7 (bits[31:16]: port1=2=GPIOB, pin1=7, afmux1=10, mode1=4=AF;pull-up;medium-speed)
However, it does not work. I also trace its ROM log. Attached is log.
Solved! Go to Solution.
2023-07-26 6:19 AM
Hi @fantasylsdo ,
I think the issue is that you are using STM32MP15x Rev B. (from a very old stock I guess) which have issue booting from most eMMC due to too short data timeout.
Please refer to ES0438.
You must use STM32MP15 Rev. Z devices.
As a workaround, few eMMC was identified as working with Rev. B (Toshiba THGBMNG5D1LBAIL, THGBMDG5D1LBAIL, and Kingston EMMC04G-M627-X03U)
Please confirm your device version looking at package marking (or printed on console log during flash programming).
Regards.
2023-07-21 9:15 AM - edited 2023-07-21 9:16 AM
Hi @fantasylsdo ,
as soon you set OTP3 to use non-default AFmux, you should define ALL the required pins by the BootROM.
Here you miss to define CLK and D0. Note: D1 is useless for eMMC at BootROM stage.
So, your OTP shoud look like:
(please double check values according to your needs)
Regards.
2023-07-24 7:50 PM
Hi Patrick. Thanks for your reply.
I have a question about OTP5: 0x10945391. The mode of CLK is configured as 1 (no pull; medium speed). But I find in this link https://community.st.com/t5/stm32-mpu-products/changing-the-emmc-pins-with-otp/td-p/155797. The mode of CLK is configured as 4 (pull up; medium speed). Does it matter?
2023-07-25 6:05 AM
HI @fantasylsdo
Internal pull-up on CLK is not so important as it is driven push-pull once initialized. Usually there is also an external pull-up.
Both configuration will work.
Regards.
2023-07-26 5:05 AM
2023-07-26 6:19 AM
Hi @fantasylsdo ,
I think the issue is that you are using STM32MP15x Rev B. (from a very old stock I guess) which have issue booting from most eMMC due to too short data timeout.
Please refer to ES0438.
You must use STM32MP15 Rev. Z devices.
As a workaround, few eMMC was identified as working with Rev. B (Toshiba THGBMNG5D1LBAIL, THGBMDG5D1LBAIL, and Kingston EMMC04G-M627-X03U)
Please confirm your device version looking at package marking (or printed on console log during flash programming).
Regards.
2023-07-26 6:24 AM
Hi Pactrick,
You are correct. I'm using STM32MP151CAD Rev.B. Thanks for your kind advice. We will consider to change STM32MP15 Rev. Z devices.
Thanks for your efficient reply again. I'll close this question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.