STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157F DDR Caching/Organization

Hello, we are currently working with the STM32MP157F-DK2 evaluation board. We have a couple questions regarding the DDR setup on the board. First, when accessing DDR memory, is there any level of CPU caching occurring, or can the memory region have c...

Bit Mapping.png
heelsec by Associate
  • 2246 Views
  • 0 replies
  • 0 kudos

switch off/on pmic

HI,Voici mon problème, Sur ma carte éléctronique, j'ulise un stm32mp15 ave le pmic de ST. J'utilise la broche LD02 du pmic pour allimenter un récépteur GPS (relié sur l'uart 7) que j'aimerai pouvoir couper/allumer (depuis le user space) pour des ques...

ABouc.1 by Associate
  • 2055 Views
  • 2 replies
  • 0 kudos

Resolved! USB HID doesn't work without hub

Hi, when I inserted keyboard/mouse to USB host port, nothing happened (log console) and this even cause usb host stop working then.But when I inserted keyboard/mouse to a hub and connect this hub to usb host port, everything working fine.The problem ...

Dat Tran by Senior II
  • 3973 Views
  • 2 replies
  • 1 kudos

STM32MP157CACxx: 32 bits LPDDR3 support?

Hello,I'm considering to use Kingston 04EM04-N3GM627 as the memory and storage for STM32MP157C/F with 32-bit LPDDR3 support. The Kingston part has 16M words × 32 bits × 8 banks, but the evaluation board uses two 16 bits memory parts. Is this Kingston...

fcl by Associate
  • 2272 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.