STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157 VREFBUF enable fails

We are using STM32MP157F in our board, running OSD32MP1 Debian SDK v3.0 (Linux Kernel v5.10-stm32mp).In our board VDDA pin is connected to LDO5 at 3.3VVREF+ and VREF- pins are connected to VSSA.We cannot supply external VREF for ADC due to hardware l...

VREF-connection.png
farid by Associate II
  • 2369 Views
  • 1 replies
  • 0 kudos

USB Gadget does not recognize disconnect

Hello,I'm kind of stuck with my STM32MP157C custom board. In general, everything works fine except for the USB. I'm using the new Ecosystem 5 and using the USB OTG with the NCM Ethernet gadget. My USB has no ID pin wired and is in peripheral mode all...

JSala.3 by Associate II
  • 3020 Views
  • 1 replies
  • 0 kudos

Resolved! Disable JTAG

Good morning,I would like to know if I can disable the JTAG in the STM32MP1. Once my project is finished I do not want this interface to be active. Is there a way to disable the JTAG/SWD interface with registers/fuses/OTP?Kind regards,Andrés

AGamb.4 by Associate III
  • 3465 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.