2023-09-20 12:51 PM
Hi, when I inserted keyboard/mouse to USB host port, nothing happened (log console) and this even cause usb host stop working then.
But when I inserted keyboard/mouse to a hub and connect this hub to usb host port, everything working fine.
The problem is only happened with hid (keyboard/mouse). When I used USB thumb drive, it works just fine, no need the hub.
The chip I used is STM32MP153 and this is custom build
Does anyone know why or any hint?
Thanks.
Solved! Go to Solution.
2023-09-21 12:03 PM
I got it working. Need to enable ochi driver in device tree.
2023-09-21 12:03 PM
I got it working. Need to enable ochi driver in device tree.
2024-03-05 2:24 AM
I have a similar error but in device mode, if I connect my board to the PC without HUB there are big chances that it wont work, but when I use a hub it always is recognise be the PC.
Which drive did you precisely enable and where? Can you load some screen captures?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.