2020-07-20 11:23 PM
Follow the steps below:
My system : Windows 10 + VMware +Ubuntu 18.04
*******************************************************************
~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.31-r0/linux-5.4.31$ make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
scripts/kconfig/conf --syncconfig Kconfig
SYSHDR arch/arm/include/generated/uapi/asm/unistd-common.h
SYSHDR arch/arm/include/generated/uapi/asm/unistd-oabi.h
SYSHDR arch/arm/include/generated/uapi/asm/unistd-eabi.h
HOSTCC scripts/dtc/dtc.o
HOSTCC scripts/dtc/flattree.o
HOSTCC scripts/dtc/fstree.o
HOSTCC scripts/dtc/data.o
HOSTCC scripts/dtc/livetree.o
HOSTCC scripts/dtc/treesource.o
HOSTCC scripts/dtc/srcpos.o
HOSTCC scripts/dtc/checks.o
HOSTCC scripts/dtc/util.o
LEX scripts/dtc/dtc-lexer.lex.c
YACC scripts/dtc/dtc-parser.tab.[ch]
HOSTCC scripts/dtc/dtc-lexer.lex.o
HOSTCC scripts/dtc/dtc-parser.tab.o
HOSTCC scripts/dtc/yamltree.o
HOSTLD scripts/dtc/dtc
HOSTCC scripts/genksyms/genksyms.o
YACC scripts/genksyms/parse.tab.[ch]
HOSTCC scripts/genksyms/parse.tab.o
LEX scripts/genksyms/lex.lex.c
HOSTCC scripts/genksyms/lex.lex.o
HOSTLD scripts/genksyms/genksyms
HOSTCC scripts/kallsyms
HOSTCC scripts/conmakehash
HOSTCC scripts/sortextable
HOSTCC scripts/asn1_compiler
HOSTCC scripts/sign-file
HOSTCC scripts/extract-cert
WRAP arch/arm/include/generated/uapi/asm/kvm_para.h
WRAP arch/arm/include/generated/uapi/asm/bitsperlong.h
WRAP arch/arm/include/generated/uapi/asm/bpf_perf_event.h
WRAP arch/arm/include/generated/uapi/asm/errno.h
WRAP arch/arm/include/generated/uapi/asm/ioctl.h
WRAP arch/arm/include/generated/uapi/asm/ipcbuf.h
WRAP arch/arm/include/generated/uapi/asm/msgbuf.h
WRAP arch/arm/include/generated/uapi/asm/param.h
WRAP arch/arm/include/generated/uapi/asm/poll.h
WRAP arch/arm/include/generated/uapi/asm/resource.h
WRAP arch/arm/include/generated/uapi/asm/sembuf.h
WRAP arch/arm/include/generated/uapi/asm/shmbuf.h
WRAP arch/arm/include/generated/uapi/asm/siginfo.h
WRAP arch/arm/include/generated/uapi/asm/socket.h
WRAP arch/arm/include/generated/uapi/asm/sockios.h
WRAP arch/arm/include/generated/uapi/asm/termbits.h
WRAP arch/arm/include/generated/uapi/asm/termios.h
WRAP arch/arm/include/generated/asm/compat.h
WRAP arch/arm/include/generated/asm/current.h
WRAP arch/arm/include/generated/asm/early_ioremap.h
WRAP arch/arm/include/generated/asm/emergency-restart.h
WRAP arch/arm/include/generated/asm/exec.h
WRAP arch/arm/include/generated/asm/extable.h
WRAP arch/arm/include/generated/asm/flat.h
WRAP arch/arm/include/generated/asm/irq_regs.h
WRAP arch/arm/include/generated/asm/kdebug.h
WRAP arch/arm/include/generated/asm/local.h
WRAP arch/arm/include/generated/asm/local64.h
WRAP arch/arm/include/generated/asm/mm-arch-hooks.h
WRAP arch/arm/include/generated/asm/mmiowb.h
WRAP arch/arm/include/generated/asm/msi.h
WRAP arch/arm/include/generated/asm/parport.h
WRAP arch/arm/include/generated/asm/preempt.h
WRAP arch/arm/include/generated/asm/seccomp.h
WRAP arch/arm/include/generated/asm/serial.h
WRAP arch/arm/include/generated/asm/trace_clock.h
WRAP arch/arm/include/generated/asm/simd.h
UPD include/config/kernel.release
UPD include/generated/uapi/linux/version.h
UPD include/generated/utsrelease.h
SYSNR arch/arm/include/generated/asm/unistd-nr.h
GEN arch/arm/include/generated/asm/mach-types.h
SYSTBL arch/arm/include/generated/calls-oabi.S
SYSTBL arch/arm/include/generated/calls-eabi.S
CC scripts/mod/empty.o
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized command line option ‘-mlittle-endian’; did you mean ‘-fconvert=little-endian’?
gcc: error: unrecognized command line option ‘-mfpu=vfp’; did you mean ‘-mcpu=’?
scripts/Makefile.build:265: recipe for target 'scripts/mod/empty.o' failed
make[1]: *** [scripts/mod/empty.o] Error 1
Makefile:1110: recipe for target 'prepare0' failed
make: *** [prepare0] Error 2
Did I miss any steps? Please help to check the problem,Thanks a lot!
2020-07-20 11:58 PM
Hi @Dhung.1
As first assumption/hint please check you have all needed packages on Host side :
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages
Olivier
2020-07-21 6:49 AM
Also verify that you have properly sourced the SDK environment variable script.
2020-10-08 5:03 AM
I have the same issue,
Did you manage to resolve the problem ?
2021-02-23 6:13 AM
Hi Guys,
somebody have solution for this issue?
Thanks
2021-02-23 6:27 AM
Hi @NNahu.1 ,
The procedure expose in our Wiki has been fully validate.
Common pitfall for people getting errors are:
Please retry carefully the procedure.
You can also refer and cross-check with more complete procedure here :
Hope it help
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.