cancel
Showing results for 
Search instead for 
Did you mean: 

Changing the RIF -> RISUP -> LTDC_CMN settings in STM32CubeMX

OKN
Associate III

Hello

I am using STM32CubeMX (ver 6.14.1) to create a Device Tree (DT) for a custom board based on the STM32MP255F-AK.

I tried to uncheck the “Secure” option for RIF -> RISUP -> LTDC_CMN in STM32CubeMX, but
the checkbox is grayed out and I cannot make the change.

 

Please tell me how to change this grayed-out checkbox.


The reason I want to change LTDC_CMN from “Secure” to “Non-Secure” is...

The following error occurs during Linux kernel boot:

 

[ 0.795347] Registering stm32-rifsc firewall controller
[ 0.800826] stm32-rifsc 42080000.bus: display-controller@48010000: Device driver will not be probed

 

After investigating, including the kernel source code, it appears the cause is that the “secure” configuration is specified for LTDC_CMN.

For now, I edited the DT directly to change it from “secure” to “non-secure,” and the above error no longer appears.


[Before change]

&rifsc {
status = “okay”;
st,protreg = <
[...]
RIFPROT(STM32MP25_RIFSC_LTDC_CMN_ID, RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_L0L1_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_L2_ID, RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_ROT_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
[...]

[After Modification]

&rifsc {
status = “okay”;
st,protreg = <
[...]
RIFPROT(STM32MP25_RIFSC_LTDC_CMN_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_L0L1_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_L2_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
RIFPROT(STM32MP25_RIFSC_LTDC_ROT_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
[...]

 

Best Regards,

--

okn

 

1 ACCEPTED SOLUTION

Accepted Solutions
OKN
Associate III

Hello

It seems the problem was caused by the A35S(OP-TEE) option being checked under Pinout&Configuration -> Multimedia -> LTDC -> Mode.

After unchecking this option, the secure option under RIF -> RISUP -> LTDC_CMN was also unchecked.

 

Best Regards.

--

okn

 

View solution in original post

2 REPLIES 2
OKN
Associate III

Hello

Regarding the issue where the “secure” checkbox for LTDC_CMN cannot be

unchecked, the cause was that the “OP-TEE” checkbox was
selected under Settings & Configuration -> Multimedia -> LTDC Features.

Best Regards,

--

okn

 

OKN
Associate III

Hello

It seems the problem was caused by the A35S(OP-TEE) option being checked under Pinout&Configuration -> Multimedia -> LTDC -> Mode.

After unchecking this option, the secure option under RIF -> RISUP -> LTDC_CMN was also unchecked.

 

Best Regards.

--

okn